Part Number: OPA857EVM-978
Firstly, I am trying to set the module into test mode to verify it's working correctly before connected a diode.
In the datasheet it species that I first must 'set the Test_SD pin to +VS' and includes a diagram:
However on the physical board, I can see no such connection! There are only the 3 SMA connections.
Where are all these other connections illustrated in the diagram?
My second question is if this product has a MINIMUM frequency that it will operate at. For example will this amplifier work with an input signal of, say 5MHz?
Kind Regards,
James