Other Parts Discussed in Thread: INA226
Hi,
Design Details:
Rshunt = 0.01ohm (CRF0805-FX-R010ELF, circled in schematic)
Max Expected Current = 4A.
Bus Voltage = 7.5V
CALIBRATION: 0x0FFF
CONFIG: 0x27FF
So current sensitivity for 1 LSB is 1mA. But I always seem to have an offset of ~20mA. In PCB layout we have a good kelvin connection to the resistor (CRF0805-FX-R010ELF). Attached is a graph of the accuracy we are getting. I've measured it using two different methods (power supply across shunt / electronic load), its always the same. I've even taken D3 out (see attached schematic) of the circuit to ensure nothing else is downstream is drawing power.
Also, one more interesting clue is that the offset tracks the bus voltage. So, I can get to a 0mA reading when VBUS = 0V. It seems like there is a resistive load on IN- to ground except my power supply current is reading 0mA?! Maybe the part is damaged?
Any ideas?
Thanks!
Erik