Other Parts Discussed in Thread: XTR117, XTR110, XTR115, XTR116
i designed a circuit which converts 8 bit digital data to 4 to 20mA transmitter. In the datasheet it is mentioned that we need to use the mosfet IRF9513.I did not had the IC in indian market. so i used an alternate ic IRF9520 in which the current raring is greater than the previous mentioned one.As a result i am not getting the exact current 4 to 20mA. i tried to adjust 4mA span adjustment thro' a potentiometer,but it didn't help.pls tell me how to solve this problem.