Hi,
I had made a simple buffer circuit from the TLC2272 (V+= 3.3V, V-=0 ) . The input to the IN+1 pin is +1.25V DC from a 100k potentiometer. The output shows the DC voltage (1.25V) + a 100mV pk-pk noise with a frequency of 1Mhz. We had to eventually add a 2.2uF capacitor to attenuate the noise to a manageable output, but this is very odd and can identify where the noise is coupling from!
Regards,
Tony