This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6643: Datasheet spec

Part Number: LMH6643

Hi

LMH6643 datasheet was changed from P-ver to Q-ver as below.

 What is meaning AT TEMPERATURE EXTREMES? Total temperature range -40C to +85C? or only -40C and +85C?

I'm confusing, because, it was deleted "at Tj=25C" on the P-ver datasheet.

So,I think, Q-ver say the right values are spec at total temperature range, and the left values are spec at only -40C and +85C.

Or The right values are spec at room temp, and the left value are spec at total temperature range.

Which Is correct?

Muk

  • Hello Muk

    Yea, National likes to make you piece it together like kind of a puzzle, 

    The P rev says change to TI format but this is not a TI format, no TI datasheet has this added over temp range column that I know of. 

    Piecing this together the recommended range table says -40 to 85C so that is the implied over temp for the temp extremes column

    The footnote 1 on the right columns says tested which would be somewhere around 25C - footnote 2 is also humorous. 

    Also note the midscale condition at the top is at 1.5V, only 0.3V of 25C positive swing from there - so not much DC coupled operating range going positive for gain of 1.