Part Number: LF398-N
Hello everyone,
I am using a LF398S8 Sample and Hold Amplifier and am trying to give it an analog signal in the range of 0-10V that the SaH should hold on logic low and sample on logic high.
I am giving it the required supply voltage of +/- 15V and am changing the logic input that I hooked up at pin 8 every 5 sec. Logic high is 5V.
Pin 7 is grounded and on pin 6 I am using a 10nF capacitor. As an anaolg input I am using 5V for testing. However once I start giving it my logic input. The output always stays at about -14V.
Can someone tell me what on my circuit went wrong or is the SaH that I am using not the correct one for this application?
I am looking forward to any help I can get.