Other Parts Discussed in Thread: TLV1702
The Above Circuit is Designed to satisfy below requirement:
1. HIGH FOUT When LED Is Normal
2. LOW FOUT When LED is Fail Open
3. LOW FOUT When LED is Fail Short
4. LOW FOUT When VCC is Disconnected
5. LOW FOUT When GND is Disconnected.
High Signal Corresponds to 10V or Higher, Low Signal Corresponds to less than 5V
The above Circuit is able to satisfy all the 1-4 Requirements.However, when the Ground is disconnected, it is reading High 12V Signal.
What Changes are required to make it LOW when GND is disconnected.