Part Number: INA303
Other Parts Discussed in Thread: INA206
As mentioned in my earlier query, I am using INA303A2 to sense overcurrent condition set at 170mA. To test this circuit I set the load current from Power supply at 180mA and gradually increase the voltage. But the supply's short LED turns on as soon as the voltage knob is moved. This even happens even if the INA303 circuit is not powered on and only the load is powered. Any idea what could be the issue?