This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM311: Suggest me a better/faster option for a comparator

Part Number: LM311
Other Parts Discussed in Thread: TLV3201

HI,

I have developed my circuit design where I adopt LM311 as a main comparator. Response time is about 200ns and I consider this as not so fast or not acceptable. Can you suggest me a comparator IC which is quite faster than this? Power supply is (0, +15VDC) and input signal is (0, +10Vmax). Everything is ground referenced.

  • Slavisa

    Unfortunately we do not have a comparator that can operate at 15V which is faster than the LM311.

    If you wish to share more details about your application, maybe we can find a solution around the high operating voltage requirement.

    Chuck

  • Thank you.

    In the meantime, I changed some details regarding power supply levels. LM311 is now at 5VDC, input levels are 0-5VDC, output 5-0VDC (inverting opamp). Offset is set in range 1-4.16VDC. Reaction time is somewhat lower. I would like to see some faster circuitry, just to compare... 

  • Our TLV3201 family is a 5V, 40ns prop delay device.  This device also has a push-pull output stage which should be better for you if the output needs to toggle frequently and level-shifting is not required.

    Chuck

  • You may want to take a look at the AD790.  It handles ±15V supplies and inputs.  Prop delay strictly less than 45ns, approaching 20ns for large input over-drives.  

    I agree that reducing the operating voltage is preferable, assuming it doesn't mess up some other aspect of your timing.  Once you need a fast comparator to operate outside of ±5V, your options become very limited.  

  • Slavisa

    Andrew's comments are fair.  There are limited choices at higher operating voltages.  Frequently such devices are used to protect against high amplitude transients and then level shift on the output to a lower voltage level.   Hopefully the information you have received will allow you to move forward.

    Chuck