Part Number: OPA549
Hi,
I try make a 60V 30A amplifier with OPA549. And I design first 5 OPA549 parallel and 1 different opamp for drive all of them. At the beggining, I do not get any problem and I used this system 1 day. After I chech all opamp one by one and I show one opmap begin 9V bias. for example I drive 1V but I show 10V, I drive -1V I show 8V. Also I drive AC signal and I show same offset. But when I use all of opamp I dont show bias.
After I change this opamp but at now the other one opamp show same error. I do not understand this. Could some one help us?
Thanks