This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR111: XTR111 Initial Accuracy

Part Number: XTR111

Hi SIR:

     I use the XTR111 input 0.8Vto 4V  to be  4mA-20mA. i find when I want ouput the 20mA it only 19.985. the error (20-19.985)/20 =0.075%  but if the output Current under the 20Ma example 19.6ma the Error (19.6-19.589) /19.6=0.056%. why the 20ma Error is bigger than under 20mA.it will effect my product Accuracy