Part Number: INA333
I have a question with regard to the Input Bias Current Return path section (8.2.2.5) of the INA333 datasheet. I am used to placing this bias current compensation resistor at the input(s) when connecting the In-Amp to a floating source (battery, thermocouple, etc.).
- Would I still need to add this resistor if the sensor I am connecting to is referenced to the same ground as the INA as shown below ?
- What if the sensor is connected at a distance (100ft) form the INA ?
I’ve asked around and am getting different answers on this, hopefully the analog gurus at TI can clue me in on this.