Other Parts Discussed in Thread: OPA172, TLV271, ADS131A02
Dear sir,
we are using AMC1300 for current measurement.
Measurement range : 0 to 75A
Shunt resistance : 1mOhm
High side voltage : 75mV
low side voltage : 615mV.
measurement signal frequency : DC-20kHz
We wish to have amplifier get the secondary side voltage as 10V. Could you please suggest the suitable amplifier to connect in the AMC1300 output circuit.
Thanks & regards,
Rajasekaran