Other Parts Discussed in Thread: OPA548
In our company we are using OPA548 for programmable power supply application purpose.We have used your Digitally-Controlled Programmable Power Supply schematics for our application refer to page number 15 of OPA548 datasheet .Whatever mentioned in that schematics ,used all IC and capacitor except resistor(used 10k and 4.12k instead of 9k,1k respectively for a gain 3.4) .
We are facing problem with OPA548 IC , IC gets very much heated after connecting to the load then it goes to the thermal shutdown within 40 second for both higher current and lower current.Without load there is not much heat in the IC.We provided heat sink to the OPA548 IC ,tried with big heat sink but still same problem.I have attached the readings taken for OPA548 output voltage.Kindly find the attachement.Can you suggest a solution for this problem.....?
For DAC, supply voltage is 5v. Reference voltage to DAC is set to -5v. For OPA548, supply voltage is 15v. OPA548 gain is set to 3.42. *Buffer output and Analog output taken without connecting to the load *Measured the values in multimeter.s *Readings taken when current digital value is set to zero and varying the voltage digital value. S.NO Digital Buffer output Analog 1. 4096 4.09/2.92 13.40 2. 2048 2.4 8.35 3. 1024 1.2 4.17 4. 512 0.6 2.08 5. 256 0.3 1.03 6. 128 0.15 0.58 7. 64 0.075 0.53 8. 32 0.037 0.51 9. 16 0.016 0.50 10. 8 0.011 0.50 11. 4 0.011 0.50 12. 2 0.011 0.50 13. 1 0.011 0.50 14. 0 0.011 0.50 *Readings taken when current digital value is set to max and varying the voltage digital value. S.NO Digital Buffer output Analog 1. 4096 4.09/3.6 13.16 2. 2048 2.4 8.35 3. 1024 1.2 4.17 4. 512 0.6 2.08 5. 256 0.3 1.03 6. 128 0.15 0.62 7. 64 0.075 0.56 8. 32 0.037 0.54 9. 16 0.016 0.54 10. 8 0.011 0.54 11. 4 0.011 0.54 12. 2 0.011 0.54 13. 1 0.011 0.54 14. 0 0.004 0.54 ******************************************************** For 12v ,digital value is 2950 For 11.87v ,digital value is 2900