Part Number: THS3217EVM
Other Parts Discussed in Thread: THS3217
Hi there,
Can I use THS3217 as a bias tee to add DC to a single-ended AWG output (e.g Vin+ for signal and Vin- for DC)? Our application prevents us from using conventional bias tee which has lower cutoff frequency higher than we want (we need the lower cutoff below 1kHz). I've tried the approach I mentioned and I can shift the signal level but the gain is pretty low after D2S (around -4dB). Although I can use OPS stage the frequency response of the EVM becomes poor when OPS is enabled.
Best wishes,
Kelly