This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-3PHGANINV: Power of the inverter

Part Number: BOOSTXL-3PHGANINV
Other Parts Discussed in Thread: LMG5200

Which is the power that the inverter can provide to me? It is based on the input voltage and the nominal current? 48 V and 7 A rms?