This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA233: Supply Current Consumption

Part Number: INA233


Hi Team, 

I am looking into the operating power consumption of INA233. From the datasheet it specifies ‘quiescent current’ and ‘Quiescent current, power-down (shutdown) mode’. The former one should refers to the current consumption at which delta-sigma engine is active, right?

How would the Iq change vs different conversion time, which is not specifies in datasheet? Would there be any other settings change that could significant impact the quiescent current?

Thanks for your help!

Peiheng.

  • Hi Peiheng,

    the given current consumption of 310µA typical and 400µA maximum should be an averaged value under normal operation including all the variable conversion times. A faster conversion might draw a somewhat higher supply current during the conversion, but at the same time the conversion lasts less. And a slower conversion might draw a somewhat lower supply current during the conversion, but at the same time the conversion lasts longer. So, I guess, that in a first order approximation changing the conversion time should not significantly change the average current consumption.

    See also figures 19...22 of datasheet. And keep in mind, that the current through the pull-up resistors at the digital lines when emitting low level will also contribute to the overall current consumption.

    Kai

  • Peiheng,

    Kai is correct here. The changes in the current based on different conversion times should be small, and counterbalanced by the differing amount of the conversion time. If you need specific, transactional Iq values for each conversion time, you will need to characterize these yourself, as we do not provide this in the datasheet. You should also note that Iq will be affected by the speed at which you perform I2C communications as well as temperature, as shown in figures 19-22 of the datasheet.

  • Kai, Carolus,

    Thanks for your prompt response!

    Peiheng.