This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA216: Is there a tool which INA216 output data can be seen on PC

Part Number: INA216


Hello,

We would like to see INA216 output in PC. INA216 is analog output product hence ADC is required.

Is there any tool a kind of below?

INA216 -> ADC -> interface -> PC(GUI)

Best regards,

Toshihiro Watanabe

  • Toshihiro-san,

    Unfortunately, TI does not make a standalone PC ADC or interface for testing products. 

    That said, I can think of a few options that might work for you here:

    1. You could look into acquiring a third party PC ADC, such as Picoscope.

    2. You could acquire a TI ADC EVM that includes a GUI for evaluation, such as the ADS7057EVM. Note I name this device for convenience. You would need to select the proper device for whatever bit-depth and sampling rate you need here for your signal, and ensure the signal chain is configured properly.

    3. You could acquire an MSP430EVM, feed the signal into an analog port, and output the measurements to a serial interface. Note though that this won't provide a graphical representation of the data, but a numerical one.