Part Number: OPA551
Other Parts Discussed in Thread: LM317, LM337
The OPA551 can source and lot of current from relatively high voltage supplies. It includes a current limit feature as well as thermal shutdown with flag.
However, it is clear from the Abs Max ratings and the SOA curve they refer to that it is still possible to damage the device if it drives a continuous short circuit (fault).
The circuit in question uses 12V/Gnd as bias to the OPA551. According to SOA curve with 12V from Vs to Vo, the part will tolerate ~60 mA before exceeding the SOA for the SOIC package.
This '551 is driving a transducer through a wiring harness and we need to mitigate the fault where the wires i the harness are shorted to ground.
Do you have any suggestions on the best way to protect the part from a short circuit on its output?