Part Number: OPA2990
Hello TI community, recently I implemented the circuit attached below on a breadboard.
The ratio of attenuation looks good but when I tested the circuit with a sine wave as input the output shows distortion near of the peaks. This starts above 30 KHz and is evident with voltages above of 5 Vpp althought I have not done many tests varying the voltage of signal input. When frequencies below 30 KHz everything looks good even with high voltage swings, simulation in TINA were ok and based on the specifications of the OPAMP it should work ok but it does not besides the frequency of the signal is not so high for a breadboard and the configuration is high input impedance so the amplifier is not loading the input signal.
I will appreciate the help to figure out what is happening, if you need more information just tell me. Thanks in advance for the attention.