Part Number: OPA548
We are using OPA548 in our design with the following requirement-
“The output current of OPA548 must be limited to 171mA.”
For this, we have used a 402k Ohm resistor as the current limit resistor (RCL). Can you suggest if there is any way in which we can avoid using a big value resistor like 402k Ohm and achieve the 171mA current limit?
Also, there is a 4.75V source internal to the OPA548 connected to a 13750 Ohm resistor as shown from the snippet attached below (from the datasheet) –
Formula for RCL shown below (from the datasheet)-
Could you also let us know how the value “15000” is derived in the formula?