Other Parts Discussed in Thread: LM393, ,
Dear Team,
Do you have the comparison table between LM2903EDR2G and LM2903DR?
https://www.onsemi.com/pub/Collateral/LM393-D.PDF
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Do you have the comparison table between LM2903EDR2G and LM2903DR?
https://www.onsemi.com/pub/Collateral/LM393-D.PDF
BR
Kevin
Hello Kevin,
See below.
Please note we are also introducing the "B" version of the LM2903/LM393 family, with improved specifications. I have added it to the table.
LM2903B samples are now available.
| OPN | LM2903EDR2G | LM2903DR | PLM2903BIDR |
| Manufacturer | ON | TI | TI |
| Pinout | OPAMP_DUAL | OPAMP_DUAL | OPAMP_DUAL |
| Channels | 2 | 2 | 2 |
| Pkg | D8 | D8 | D8 |
| Tmin | -40 | -40 | -40 |
| Tmax | 105 | 125 | 125 |
| VccMin | 2 | 2 | 3 |
| VccMax | 36 | 36 | 38 |
| Tresp (us) | 1.500 | 1.300 | 1.000 |
| Is Max Ch (uA) | 500 | 500 | 200 |
| InRange | To V- | To V- | To V- |
| OutRange | OC | OC | OC |
| VosTyp (mV) | 2 | 2 | 0.37 |
| VosRmMax (mV) | 7 | 7 | 4 |
| IbiasTyp (nA) | 20 | 25 | 15 |