Part Number: INA240
Hi,
customer are usins INA240A1 to replace AD8210 to do current sensing for motor drives.
when no PWM, INA240A1 performs better; when here is PWM, the accuracy changed a lot, worse than AD8210. f=10kHz. here is sch and waveforms:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA240
Hi,
customer are usins INA240A1 to replace AD8210 to do current sensing for motor drives.
when no PWM, INA240A1 performs better; when here is PWM, the accuracy changed a lot, worse than AD8210. f=10kHz. here is sch and waveforms:
Hi Yuan,
Are “Ib” and “Ia” for AD part and INA240 respectively?
It appears the differential input is 0V, with the common mode voltage being chopped. At 10KHz, the period is 100uS, how is the 200uS sampling period synchronized with the PWM? What is the wait time after each PWM transition?
Also what is the value of the shunt?
In addition, the 470nF cap is fairly large comparing to the 22Ohm, the output might be slightly oscillating, please check. The combination can probably be adjusted to 100nF and 150Ohm.
Regards, Guang
Hi Yuan,
Looks like this issue is being addressed in another thread, lets close this one.
Regards, Guang