This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9062: Different Foot Print

Part Number: TLV9062

Dear Team,

Do we have TLV9062IDGKR with footprint width 0.5mm?

Because of the customer using the wrong footprint VSSOP(0.5mm) but it should be DGK (0.65mm)

Or you have a suitable device to replace?

BR

Kevin

  • Hi Kevin,

    DGK is the same as VSSOP for TLV9062. Your customer is using the correct package. The body size of DGK (VSSOP) is 3.0mm x 3.0mm and the package size is 3.0mm x 4.9mm. Our smallest package size is single channel X2SON with a size of 0.8mm x 0.8mm.  I hope this helps!

    Best Regards,

    Bala Ravi