Would I be able to find op-amps and transistors that are able to handle 8-12T magnetic field?
I want to design an pre-amplifier circuit that needs to be placed inside a uniform 8-12T magnetic field without disturbing the uniformity of the field (so I can't use shielding techniques). I am having trouble sourcing components, since datasheets don't usually have any information about the components' behaviour in magnetic fields.
The signal I wish to amplify is in the RF range, and the gain should be at least 30dB. It would be ideal to find an op-amp that can operate in these conditions but it would also be great to get recommendations on any transistors as well.
Maybe a list of transistors/op-amps with the least amount of metal/ferromagnetic/paramagnetic/magnetoresistive materials? I've read some papers about the transistors' geometry helping their functionalities in strong magnetic fields, however, it was difficult for me to understand/find any information about how the transistors are manufactured, etc.
Thank you so much for the help!!