Other Parts Discussed in Thread: OPA333, ISO1541, INA220
Hello, I also want to use INA226 to sense voltage higher than 36V (max 58V ). Is there any easier way to do that instead of adding OPA333 and fets?
we don't need a very precise current read so maybe just an equal voltage divider on Vin+ and Vin-?
We changed the voltage of the system to 48V when it was 30V before and we missed that part....the gerbers are almost out so I need the simplest/fastest solution. I added a voltage divider on Vbus but forget about Vin+ and Vin-.
Any suggestion to help?
Thanks