Part Number: INA226
Other Parts Discussed in Thread: INA3221
I have a client looking for something similar to the INA226 features ( I2C capable/16bit resolution ) but I needed more features listed below:
- 16bit resolution.
- Bus voltage can read 100V max ( if none, 40Vmax is okay )
- >2 channels, I need 3minimum channels.
- High impedance input.
- Has reset capability.
- 3.3V supply.
Or can you recommend something similar to LTC1859 ( but I need high impedance Mux input ) with the following features
- 16bit resolution.
- MUX input channel can accept >10V
- =/>4 channels.
- High impedance input.
- Has reset capability.
- 3.3V supply.
- I2C/SPI capable
Thank you for helping me.