Part Number: USB2ANY
Other Parts Discussed in Thread: CODELOADER, , LMK03328
I have the USB2ANY module. I installed the Codeloader 4 software. The module firmware has been downloaded to the module and on the
port tab of the GUI I can click the Identify button and the LED on the module blinks. On the pin configuration I have tried to use SCL as Clock bit 1 and Data bit as 2 and vice versa and set the I2C address to my target address 0x54, I have the Select Device as the LMK03328, my target. But I do not see any activity at all on the SCL or SDA on the scope, they always remain at +3.3V when I try and search for I2C devices or read all registers. I need to determine if my LMK03328 EEPROM is misprogrammed today.