This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC3301: AMC3301 error analysis

Part Number: AMC3301
Other Parts Discussed in Thread: ISO224, AMC1311

Hi

I would like to use AMC3301 for high voltage measurement with resistive divider network and its thevinin's equivalent voltage at maximum measurement voltage is 250mV with 10kohm thevenin resistance.

What would be the output error voltage due to input bias currents?

What would be the gain error due to input thevenin impedance(source impedance)?

How to compensate if the above errors are significant?

Regards,

Naveen.