Part Number: INA3221
Other Parts Discussed in Thread: INA219, INA138
I use the PAC1934 to monitor currents and voltages on rails with relatively high impedance (1k or so). I found that it creates very fast transients on the signal when its ADC samples the inputs. This is not acceptable in my circuit and it was not possible to reduce this to an acceptable value by the suggested filtering measures (series resistors, parallel cap).
Is the INA3221 better in this respect? Or do I have to use a part like the INA219, which has a PGA in front of the ADC, for which reason I wouldn't expect any such kickback noise.