Other Parts Discussed in Thread: DRV8436E, INA186, INA240
Hi Amp team,
In case of customer want to monitor the motor current by MCU,
We are recommending sense resistor in series with the motor coil winding between H-bridge as current monitor solution to my customer.
Latest our motor driver have integrated current sense for current control (for example 2ch DRV8436E).
PGND current sense is not acceptable, because it is connected to other internal circuit.
Could you please give me your recommended current sensing solution?
I will propose the following device. However, it may be over spec(little bit expensive).
Customer want to use the general opamp as possible. (please let me know the schematics for bi-directional current sense solution with general opamp)
Conditions
VM=24V
IM= max 3~4A (Bi-directional current)
Muk