Part Number: XTR300
Hello there,
Hope you are doing well.
In one of my system i want to use two XTR300 (one for voltage output and one for current output).
Those both XTR300 will be operated from the same power supply . I have different choice from below options. But to make it lower cost (assume that less current will be lower cost for me)
1) +-12v (+-33mA)
2) +-12v(+-43mA)
3) +-12v(+-75mA)
4) +-12v(+-83mA)
5) +-12v(+-100mA)
1) +-15v(+-25mA)
2) +-15v(+-33mA)
3) +-15v(+-43mA)
4) +-15v(+-83mA).
in the datasheet supply input current shows +-25mA. But still i want to confirm that is it maximum current xtr300 needs to operate on full scale ?
Thanks,
Bhautik