This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA-TI: Stepping Parameters

Part Number: TINA-TI


When doing parameter stepping of several components at the same time is there a way to tell, which trace uses what parameter values by part ref des?  I know you can click on a trace and it will give a list of values used for that trace but it does not tell you which part was at what value.  I have multiple parts using the same list of values and cannot tell which part was at which value for the particular trace.

Right now I get "VM1[8]: 15.55k[Ohm] 505.9[Ohm] 505.9[Ohm] 15.55k[Ohm]"  Would like something like "VM1[8]: R1=15.55k[Ohm] R2=505.9[Ohm] R3=505.9[Ohm] R4=15.55k[Ohm]".

Hope this question makes sense