Part Number: PGA308
Hi,
Software Lock Mode What exactly is the task of Control Bits mode? I didn't get the full information in the data sheets.
Mert
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mert,
The PGA308 has different modes of operation as discussed on Chapter 5 of the PGA308 User Guide: One-Wire Write Mode, One-Wire Read Mode, OTP Program Mode, Standalone Mode, 1W Connected to VOUT Program Mode, Virtual Software Lock Mode, Software Lock Mode, and Shutdown mode.
When setting the SWL[2:0] register to '101' allows you direct Read/Write RAM register control of the PGA308 in the Software Lock Mode:
Software Lock Mode allows you to control the PGA308 RAM directly by enabling the One-Wire interface, disabling any One-Wire timeouts, and disabling the checksum check normally performed between the CHSR Register and CHKS Register. This mode is designed for microcontroller control of the PGA308 through a microcontroller UART interface. It allows the PGA308 to be controlled as a flexible data acquisition front-end.
The user can select to load the settings of one of the seven OTP user banks and load them into RAM; and/or the user can program the RAM contents directly. To access this mode, the SWL[2:0] register must be set to '101' as shown on table 7-44 (other settings of SWL registers default to standalone OTP mode, and the POR value of this register is '000'). Please refer to pages 72-74 of the PGA308 User Guide, and the flow diagram on page 73 (figure 5-14).
Thank you and Regards,
Luis
Hi Luis,
When calibrating with the PGA308 USB DAQ board, SWL [2: 0] will be set to ABA. After the calibration process, SWL [2: 0] will be set to AAA and OTP will be loaded. I wonder if I understood the right.
Thank you.