Part Number: OPA2990
Other Parts Discussed in Thread: OPA2170
Hi,
we can need the OPA2990 but in the VSSOP (8) package.
Greetings
George
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi George,
The OPA2990 in the 8 pin VSSOP package is not currently in our schedule so it may be a year or more before the device is released in that package. The shutdown version of the device, OPA2990S, will RTM in the 10 pin VSSOP package and is currently available in preproduction samples.
Thank you,
Tim Claycomb
Hi George,
Would the 10 pin VSSOP package work for you? You could connect the shutdown pins of the device so the amplifiers are always enabled.
We also offer the OPA2170 in the 8 pin VSSOP package which is a close cross to the OPA2990. Would the OPA2170 work for you?
Thank you,
Tim Claycomb
Hi Tim,
I use now the OPA2170 with the 8 pin VSSOP. I will change it due to more output current ability of the OPA2990 (80mA/-80mA at OPA2990 against to 17mA/-20mA at OPA2170) without need to change also the PCB.
Thank you
George
Hi George,
Thank you for your interest in the OPA2990. If you need any additional support please let me know.
Thanks,
Tim Claycomb