Since working with low intensity light I need to increase the responsivity. Rext= 50 MOhm gives me desired voltage responsivity but it will lead to a 3 dB rolloff at 340 Hz, well less than the desired 5 kHz bandwidth. Could it possible to use the second stage to wider bandwidth, i.e. a differentiating amplifier whose input RC combination is chosen to match the RC product of the feedback impedance in the OPT101 amplifier stage. The second stage’s feedback RC combination will be smaller, which serves as frequency compensation. The second stage will acts to restore the frequency response of the circuit. Will it help? A plan to use the TLE2071A.