Part Number: INA333
I've employed an INA333 to amplify a strain gauge's signal. I'm testing with screw 2 of the J2 screw terminal tied to 0.515V supply, and screw 3 tied to GND, rest is as shown.
the INA333 is giving me an output of 3.48V, doing the math (1+(100kohm/0.39kohm))×0.515V = 132.6V so I should be seeing V+ of 5V. I checked the supply voltage and reference voltage, both are where they should be, and adjusting the signal voltage on screw 2 up and down drives the INA333 output up and down as well, just with a significantly smaller gain than what was expected.
Where's my mistake?
Datasheet for reference: www.ti.com/.../ina333.pdf
Edit: turns out one cannot simply paste an image into the text box.