Part Number: TLV7011
Hi All,
I am planning on using this part in a logic level shifting application. I detect the input voltage via a high impedance resistor divider. Due to the nature of my input levels, there is a chance that I can exceed VDD and VEE levels of the component.
Datasheet says: "Input terminals are diode-clamped to VEE. Input signals that can swing 0.3V below VEE must be current-limited to 10mA or less."
Since my sense path is high impedance, I don't exceed the current limit when I go below Vee and turn the internal diode ON. However datasheet does not mention a protection diode from input to VDD. In spice simulations I see that the input is clamped to VDD when the input signal gets too high though, so I suspect there is a protection diode on that pin as well.
Do you have any information on this? I think since my path limits the current to less than 1mA I should not need any additional protection even when the input tries to exceed VDD. Do you agree?
Kind regards,
Zack.S.