This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS7376: The solution for targeting less than 2.5 ns of rise and fall time

Part Number: THS7376
Other Parts Discussed in Thread: THS7373,

Hi Team,

Follow up the questions as below link:

https://e2e.ti.com/support/amplifiers/f/14/t/835693?tisearch=e2e-sitesearch&keymatch=THS7372

We found other Video Amplifier on TI Web. THS7373/7364/7365/7368

It looks 7373 is better than 7376 you suggest. Can you help confirm it? Which one is the best solution for us, 7373/7376/7364/7365/7368?

 

Thanks

  • Hi Team,

    Please help.

    Thanks

  • Hello Daniel,

      I looked at the previous thread. If you are bypassing the filters as Jacob suggested, then THS7373 has a higher bandwidth and slewrate. THS7373 would be the better solution if you are still concerned about rise times. It is pin compatible with the THS7376, so it would be a very easy change. I also viewed your schematic from the previous thread, and I would not suggest the 7364/7365/7386 for your application since you do not seem to need the 6-channel. 

    Thank you,

    Sima