Part Number: LMC6484
It appears from testing our design that the output resistance of the LMC6484 opamp varies when the opamp reaches saturation.
In our application we have configured the opamp as a follower and have 270 ohm seried resistor connected to the output to a successive approximation ADC. As the opamp reaches saturation the voltage at the output of the opamp (measured by ADC) is non-linear (lagging).
We are using a MAX1230 ADC from Maxim that specified input resistance should be limited to <300 ohms and I suspect that the opamp output resistance is exceeding this resulting in non-linearity on measurement. <300 ohms is required because the ADC contains a capacitor on the input that must be charged during TRACK/HOLD cycle so that the input voltage is SAMPLED and measured correctly.
The LMC6484 opamp specifies approx. 110 ohms output resistance at Vs=5V. Can you confirm that the effect we are seeing is a result of increase in output resistance as the opamp saturates?
We are seeing non-linearity between 4.7 and 4.8V which recovers beyond 4.9V. Can you confirm that this change in output resistance will only happen in this range, close to saturation?