Part Number: LPV511
Hi,
I was referring to the LPV511 datasheet, output swing high is 100mV, with Positive rail supply 3V, 3 - 0.1 = 2.9V which looks correct. For output swing low its -100mV negative rail supply is 0. The output should be +100mV, but the unit mentioned is V. The unit is datasheet is the mistake or I am reading the datasheet wrong?
Regards
Ashok