This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO224: Internal Charge Pump

Part Number: ISO224

Hi team,

According to below thread, ISO224 has internal charge pump so that ISO224 can accept bipolar input with only positive supply.

https://e2e.ti.com/support/amplifiers/f/14/p/812576/3010455?tisearch=e2e-sitesearch&keymatch=ISO224#3010455

Since ISO224 can accept ±12V with VDD1=4.5~18V, power tree seems to be following.

Is this understanding correct?

VDD1 4.5~18V → Reg 4.5V → Charge Pump(Boost ) about 15~18V for powering amplifier 

                                               → Charge Pump(Inverting) about -15~-18V for powering amplifier

Best regards,

Shota Mago