Part Number: XTR305
Hi,
How should we calculate Cc(Compensation capacitor) value?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XTR305
Hi,
How should we calculate Cc(Compensation capacitor) value?
Best Regards,
Kuramochi
Hi Kuramochi,
The procedure to estimate the compensation capacitor is discussed on section 8.2.2.6.
Is the device used in Current mode or voltage mode?
Essentially, in current output mode, loop compensation is not critical, even for large capacitive loads. However, in voltage output mode, the capacitive load, together with the source impedance and the impedance of the protection circuit, generates additional phase lag. The IA input might also be protected by a low-pass filter that influences phase in the closed loop. There is an XTR305 TINA model available on the web that could be used to assist/ perform stability analysis for the XTR305.
XTR305 TINA Spice model:
http://www.ti.com/product/XTR305/toolssoftware
If you require additional assistance, please provide the complete schematic, including the XTR305 load impedance and source impedance characteristics and the XTR305 settings (voltage mode or current mode), and we could advise/support.
Thank you and Regards,
Luis
Hi Kuramochi again,
in a standard application the circuit of figure 40 is recommended. And if an output protection is needed, add the diodes from figure 46.
Kai