Part Number: LPV511
Hi,
We have selected LPV511 OP-AMP for High Side Current Sensing . We require the following confirmation before proceeding,
1.Is the resistor R3 Internal/External to the IC? I assume as per the datasheet it is internal and has a fixed value of 10K which cannot be varied by the designer. Please confirm!
2.There is no need for a feedback resistor and we require only 3 resistors R1,R2 and R3 for proper current sensing as per the application circuit.
3. What is the min and max gain that we can configure with LPV511?
4.Can we configure gain for 1.366 when R3=10K and R2 = R1=7.32k and Gain of 50 when R3=10k and R1=R2=200E?