This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6611: Absolute Maximum Ratings : VIN Differential

Part Number: LMH6611
Other Parts Discussed in Thread: LMH6639

Hi Team,

I would like to know the Absolute Maximum Ratings "VIN Differential" specified value of LMH6611/2.

For example, I found that the LMH6639 data sheet has Absolute Maximum Ratings  value of ±2.5V.

As shown in Figure 44 of the LMH6639 datasheet, the diode is bi-directionally connected to IN+/IN-,

so it understands that the specified value is set.

In this configuration, LMH6611/2 also has a bidirectional diode inside IN+/IN-. (Data sheet Figure 67)

Thank you and Regards,

Kenji