Other Parts Discussed in Thread: TLV3201-Q1,
Hello,
I have two questions on propagation delay time specs of TLV3201-Q1 or TLV3202-Q1.
- TLV3201-Q1 or TLV3202-Q1's data sheet specifies its propagation delay times, tPD, but what's the voltage level condition for the specs? I guess it's either the start of rise/fall time, the end of rise/time, or the middle (50%) of the output voltage swing.
- For the specs under full temperature range, TA = -40 to 125 °C, what are the conditions of input overdrive and CL?
Best regards,
Shinichi Yokota