Other Parts Discussed in Thread: INA190, INA226
Hi,
I want to measure 0 to 60A current across Low side 250 uOhm 5W shunt resistor.My ADC is 10bit and max 3.3V. which would be the beast part for this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Pritesh,
Thank you for posting your question.
You most likely want a current sense amplifier (CSA) with the lowest offset. The INA190 has the lowest offset (±15uV). I would recommend starting with the INA190A4 (200 V/V). So at 60A the shunt voltage is 60*250µ = 15mV, which the INA190A3 would amplify to 15mV*200V/V = 3V.
You could use the circuit example to understand how to maximize INA190 dynamic range and calculate maximum possible error.
http://www.ti.com/lit/an/sboa336/sboa336.pdf
You could also use a digital device such as INA226 which has a ±10uV max, but it seems you need an analog device.
Hope this helps.
Peter