Part Number: OPA4277-EP
Other Parts Discussed in Thread: OPA4277,
We are having one design using OPA4277. In our application, we use +6V/-6V power supply to OPA4277, it's a simple DC inverter and level shifting circuit. Due to heavily capacitance (0.2uF) load applied at OP output (VVA_VP and VVA_VS see the schematic), it has instability issue (oscillation), and caused high current (up to 35mA). We realize it's a design error. Unfortunately we already made some units and shipped, and we need provide worst case and impact analysis.
Our thermal engineer is doing junction temperature analysis for different operation condition. We hope the device will work below the max junction temperature limiting.
Since we don’t have the OPA4277 internal schematic, we want to know, assume if the junction temperature exceed the max limit of +125ºC, what failure mode will be? Will it fail in shorting or open mode in +6V/-6V rail?