This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LOG114: LOG 114 with Input current upto 7mA

Part Number: LOG114


Hi,

We are using Log114 in Insulation resistance application.

Input current can increase up to 7mA DC.

It is mentioned in datasheet that input current > 3.5mA reduces the linearity of LOG114. 

1) Does the linearity reduction is permanent.

2) If yes can any one help in using LOG114 for this much input current without permanently damaging the linearity of LOG114.

  With Best Regards

 Pravin Khisti