Part Number: TLV8541
I am using the TI TLV8541DBVR in the circuit below. As you can see the + pin is ground referenced and the – pin is an AC waveform that swings above and below ground. Is this a legitimate use of the op amp? I have a physical circuit and it’s working but was wondering if the circuit is good with having an input go below ground and that the op amp sees this as an acceptable input to flip the output